Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can I run multiple GDB Instances within e2 studio?

Latest Updated:01/14/2017

Question:

Can I run multiple instances of the debugger, GDB, within e2 studio?

Answer:

Yes you can. The below description document shows how.

Multiple GDB Instances while using E2Studio.pdf

Suitable Products
e2 studio
SSP