Skip to main content
Renesas Singapore - Knowledgebase

What can be done to prevent F861 No EXT_TABLE specifier" as output?

Latest Updated:12/01/2011


When I add the -zf option and perform compilation to create a program to be placed into the internal flash FROM, "F861 No EXT_TABLE specifier" is output.
What can be done to prevent this?


The -zf option is used only when creating a program that supports self-programming of the internal flash ROM.
To make the program that writen into the internal flash ROM by using a flash programmer, set the -zf option to OFF.
Suitable Products