Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Which of the RL78 family libraries supports RL78 MCUs?

Last Updated:03/06/2017

Question:

I want to check which RL78 MCUs the following libraries for the RL78 family support.

  • Flash Self Programming Library Type01
  • Data Flash Library Type04
  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02

Answer:

For all the supported devices, see Self RAM list of Flash Self-Programming Library for RL78 Family at here.

 

Suitable Products

Flash Self Programming Libraries
Data Flash Libraries