Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What record types does MM generate from mask file in Motorola S format?

Latest Updated:09/15/2006

Question:

What record types does MM generate from the mask file in the Motorola S format?

Answer:

MM generates the following records: S1, S2, S3, S7, S8, and S9.
However, when the specified hexadecimal data file is Motorola S format and includes an S0 record, MM generates the S0 record in the mask file as well.
 
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering