Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is the maximum value returned with float division 38th power of +10 ?

Latest Updated:12/01/2011

Question:

What is the maximum value that can be returned with float division (fdiv)?
Is it the 38th power of +10 ?

Answer:

Yes, it is this size.
The return value is the range of float values described in "Table 2-3 Basic Types List" in the User's Manual (Language).
Suitable Products