Skip to main content
Renesas Singapore - Knowledgebase

Is it OK to confirm data which MM filled in unused area of the mask file?

Latest Updated:09/15/2006


I want to confirm the data which MM filled in the unused area of the mask file. Is it possible?


No, it is not. You cannot see the data from the mask file before the mask is executed. We will provide you with the dump list of your mask file when we proceed with the mask generation. We recommend that you check the data with this dump list.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering