Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to properly set up the startup routine in compiler option?

Latest Updated:12/01/2011

Question:

I want to set the startup routine in the compiler option setting dialog box from the Project Manager, but the setting items are dimmed and cannot be set.

Answer:

When any of the source files is selected in the left-side window of Project Manager (PM32 Project Window), the mode for setting individual source options is enabled, and as a result the startup routine cannot be set.
Please perform the compiler option settings after clicking a part other than the source file name in order to deselect the source file name, and then perform the compiler option settings.
Suitable Products