Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to fix errors I got when I used Intel HEX file created with IAR's tool?

Latest Updated:09/15/2006

Question:

When I use an Intel HEX file created with IAR's development tool, I get a warning that there are multiple end records. How can I fix this?

Answer:

NTEL HEX files in accordance to the contents of the option.
When using MM, specify the following IAR linker options.
- For Embedded Workbench
In [Project Option Settings], go to the Linker (XLINK) specification option and select [End only with :00000001FF] as the [Format variant] output file option.
- For Command Line
Select the [-Y0] option when starting up the linker (XLINK)

By specifying the above selections, the end record output from the Intel HEX file will be [:00000001FF]. This will prevent the "multiple end records" warning from being generated when using Intel HEX files with MM.

Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering