Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to find voltage detection setting on IO Wizard if its available?

Latest Updated:09/04/2009

Question:

I could not find voltage detection setting on IO Wizard although the MCU data sheets stated it is available for my target MCU.

Answer:

Present IO Wizard does not support voltage detection circuit setting.
Suitable Products
  • Was this article helpful?