Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to execute the command code to run a batch file?

Latest Updated:10/19/2009

Question:

When I execute the following command code to run a batch file, the "Too many parameters" error is generated.
>FL C:¥¥Program Files¥¥Renesas¥¥tutorial.abs

Answer:

If a space is included in the file path, the command will not be correctly recognized. Change the file path specification method as shown below, according to whether TCL (Tool Command Language) is Enable/Disable.

  1. When TCL is disable, and
    >tcl(ret)
    >tcl disable

    >FL "C:¥Program Files¥Renesas¥tutorial.abs"
     
  2. When TCL is enable, and
    >tcl(ret)
    >tcl enable

    >FL ¥"C:¥¥Program Files¥¥Renesas¥¥tutorial.abs¥"
Suitable Products
Simulator Debugger for SuperH Family [for High-performance Embedded Workshop]
Simulator Debugger for M16C Series and R8C Family [for High-performance Embedded Workshop]
Simulator Debugger for R32C Series [for High-performance Embedded Workshop]
Simulator Debugger for M32C Series [for High-performance Embedded Workshop]
Simulator Debugger for H8SX, H8S, and H8 Families [for High-performance Embedded Workshop]
Simulator Debugger for 740 Family [for High-performance Embedded Workshop]
E10A-USB
E8a
E10T-USB
E30A
E10A
E10T
E8
E7
M30870T2-CPE
M30850T3-CPE
M3062PT3-CPE
M3028BT2-CPE
R0E521000CPE00
R0E436640CPE00
M38000T2-CPE
E100
E200F
E6000H
E6000
PC7501
PC4701U
R8C UART Monitor Program
M32C M16C UART Monitor Program