Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to deal with this error message "Can't create Mask file"?

Latest Updated:09/15/2006

Question:

I am getting the error message "Can't create Mask file". How should I deal with it?

Answer:

Either the directory in which the mask file is created is not write-enabled, or there isn't enough space on the hard disk. Please check both possibilities and take the appropriate measures.
 
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering