Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to change settings of security information with the FlashSetInfo?

Latest Updated:02/01/2009

Question:

Is it possible to change the setting of the security information with the FlashSetInfo function?

Answer:

The setting of security information can be changed to "prohibit" from "enable" with the FlashSetInfo function.
But, the setting of security information can not be changed to "enable" from "prohibit".

<For referencce>
 Flash Memory Self-Programming Library
  V850 Microcontrollers Type 01 [Ver.5.00]
   U18208EJ3V0UM00(3rd edtion)
    5.1.7 FlashSetfInfo function

  V850 Microcontrollers Type 03 [Ver.2.00]
   U18211EJ2V0UM00(2nd edition)
    5.1.6 FlashSetInfo function
Suitable Products
V850 Family