How to build a program using the CA850 (Project Manager)?
Latest Updated:12/01/2011
Question:
I built a sample program using the CA850 (Project Manager).
When a _reset label is defined in the startup module, the following message is displayed. Why is this message displayed?
Is _reset a reserved word or is it defined in a library, etc.?
When a _reset label is defined in the startup module, the following message is displayed. Why is this message displayed?
Is _reset a reserved word or is it defined in a library, etc.?
Answer:
_reset is not used in the CA850 but is used in the RX850.
We advise you not to use this symbol.
We advise you not to use this symbol.
Suitable Products