Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Does MM register incorrect hexadecimal data in mask files?

Latest Updated:09/15/2006

Question:

Does MM register incorrect hexadecimal data in mask files?

Answer:

With MM, immediately after a mask file has been created, data is checked to see hexadecimal data registered in the mask file it created matches the hexadecimal data file originally specified.
If unmatching data is detected, an error message is displayed.
Accordingly, with MM, if the mask file is created without any error message being displayed, then the data comparison check ended successfully as well.
With MM, sampled mask data can be checked using the hexadecimal data sample feature, therefore it is possible to compare mask file content.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering