Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Does MM manipulate hexadecimal data files?

Latest Updated:09/15/2006

Question:

Does MM manipulate hexadecimal data files?

Answer:

MM only converts the specified hexadecimal data file into Motorola S format and registers it in a mask file. It does not manipulate the data in the hexadecimal data file at all.
In fact, when the specified hexadecimal data file is already in Motorola S format, the mask file is set without any manipulation whatsoever. Accordingly, if incorrect data (i.e.: RAM area data, etc.) is registered in the hexadecimal data file to be masked, it will be registered unchanged in the mask file. In such case, an error will be detected when the mask file is inspected and you will have to create the mask file again. Check the >hexadecimal data file contains the correct data beforehand.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering