Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Comment for Describing User Code of Code Generator Tool Output File

Last Updated:02/21/2018

Question:

The interrupt functions created using a code generator do not seem to have the comment for describing user code of the code generator tool. Does this mean the comment for describing is not available for interrupt functions?
Is there any way to inhibit overwriting the interrupt functions?

/* Start user code. Do not edit comment generated here */
/* End user code. Do not edit comment generated here */
 

Answer:

The interrupt functions created using a code generator do not have the comment for describing, and overwriting of interrupt functions cannot be suppressed.

The callback function is being called for user processing from the interrupt function. Describe the processing in the callback function for user processing.

You can also describe the interrupt handler by selecting “Output only initialization API function” in [Output control of API function] from the code generator property.
In addition, refer to the FAQ below.

FAQNo:1011802
How to keep the code changed?

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator