Skip to main content
Renesas Singapore - Knowledgebase

Can you provide the header file of RL78/G13?

Latest Updated:07/31/2013


I want to use the RL78/G13, but I can't find a header file that defines the on-chip peripheral functions (SFR) on the website.
Can you provide the header file?


In the RL78 Family, on-chip peripheral functions are defined in device file format, which is installed when CubeSuite+ is installed. Therefore, it is not necessary to prepare a separate header file.
When programming using an assembler (RA78K0R), program using the register names shown in the hardware manual.
When programming using a C compiler (CA78K0R), write #pragmaSFR at the beginning of the program to be able to use register names in the program.
Suitable Products
RL78 Family