Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can I generate an Intel HEX file with the MM?

Latest Updated:09/15/2006

Question:

Can I generate an Intel HEX file with the MM?

Answer:

Hexadecimal data in Intel HEX format and expanded Intel HEX format can be extracted from the mask file in Version 3.00 or later.
 
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering