Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

The value of an event flag is cleared after an event occurs

Last Updated:03/22/2017

Question:

Why is the value of an event flag cleared after the corresponding event of the event flag occurs?

Answer:

When "TS_CLR" is specified as the attribute of an event flag, the value of an event flag is cleared after the corresponding event occurs.
Suitable Products
HI7000/4 Real-time OS for SuperH Family