Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Simulator stops with the INT instruction

Last Updated:03/22/2017

Question:

When debugging is executed with the simulator, it stops when the INT instruction is executed.

Answer:

It’s the simulator setting issue. Since the default setting of simulator is “Stops with the INT instruction exception”, you may need to change it. In the RI600V4 sample project, it’s been set not to stop with the INT instruction.
Suitable Products
RI600V4