Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Robustness of handling interrupts with RI600V4

Last Updated:03/22/2017

Question:

Has the RI600V4 been designed with the algorithm which can handle frequent interrupts? I know that an interrupt which requires much time to be handled is unable to be implemented, so let me know if there is an index to handle it.

Answer:

In theory, the RI600V4 has been designed to handle frequent interrupts. However, in practice, they may delay task operation or consume CPU power, and the task may not run at all. To avoid this,we recommend not to program frequent interrupts and an interrupt requiring much time for processing.
Suitable Products
RI600V4