Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Will I be able to use the device on E10A-USB even after I add the new group?

Latest Updated:07/24/2008

Question:

When I use the E10A-USB Licence Tool for Device Group Additions, will I still be able to use the first device group registered on the E10A-USB emulator even after I add the new group?

Answer:

The E10A-USB emulator retains two types of information.

  1. Information concerning the device groups that can be used
  2. Information for communication with the target device group to be debugged

The Licence Tool for Device Group Additions only adds the information described in #1 above. The E10A-USB emulator cannot retain the information in #2 above for more than one device group at the same time.

Therefore, to change the target device group to be debugged, the user must rewrite the information described in #2 above. To rewrite this information, the setup tool must be executed.
For details on how to use the setup tool, see E10A-USB/Installation and Setup Page.

In other words, the target device group to be debugged can be changed by executing the setup tool. The Licence Tool for Device Group Additions is a tool used for enabling this change.

Suitable Products
E10A-USB