Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Influence when signal of NC (non-connect) pin of emulator is inserted

Last Updated:09/27/2017

Question:

Is an emulator (E10A, E10A-USB, E10T, E10T-USB, SDI emulator, E7, E8, or E8a emulator) adversely affected in anyway if a signal is input to the NC (non-connect) pin on the connector?

Answer:

The NC pin on the connectors of emulators E10A, E10A-USB, E10T, E10T-USB, SDI, E7, E8, and E8a, is equipped for internal-use by the emulator as well as for future extensions. Sending a signal from the user board to this pin will cause interference with the emulator's output signal, resulting in not only faulty operations, but also possible damage to the emulator itself. We strongly recommend you do not connect anything to the NC pin. If this pin is used, emulator 

Suitable Product

E10A-USB
E8a
E10T-USB
M32100T-EZ-E
M32100T5-SDI-E
E10A
E10T
E8
E7
M32100T3-SDI-E
M32100T2-SDI-E
M32100T-SDI-E