How to retrieve an ID code when using the E1, E20, E8a or E8(discontinued product)
Last Updated:04/26/2017
Question:
Are there any methods for retrieving an ID code when using On-Chip Debugging Emulator the E1, E20, E8a or E8(discontinued product) (applies to M16C, incl. R32C, and R8C Family MCUs)?
Answer:
In some cases, the ID code can be retrieved. Refer to the following instructions.
Instructions : M16C_APN_ID_110607e.pdf(332KB)
Refer to the following FAQ for the specification of the ID code.
FAQ No. | Suitable Emulator | Description |
106887 | E1, E20, E8a | How to handle ID codes |
106937 | E8 (discontinued product) | How to handle ID codes |
101717 | E1, E20, E8a E8 (discontinued product) E7 (discontinued product) | What should I enter in the dialog box asking for an ID code? |
106426 | E1, E20, E8a E8 (discontinued product) | ID code error appears |
Suitable Products
E1 [R0E000010KCE00] |
E20 [R0E000200KCT00] |
E8a |
E8 |