Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to install emulator control program without CD-ROM

Last Updated:09/27/2017

Question:

I have lost the CD-ROM that came with the emulator when I purchased it. How can I install the emulator without the CD-ROM?

Answer:

The emulator software, trial version compiler and other tools included on the CD-ROM can be downloaded from the following site.

https://www.renesas.com/search/keyword-search.html#genre=tooldownload
 

On the left side of the screen, select [Software and Tools] → [Emulation and Debugging], and download the necessary emulator control program.

Suitable Products

E1[R0E000010KCE00]
E20[R0E000200KCT00]
E10A-USB
E8a
E10T-USB
E8
E100
E200F
E6000H
PC7501
  • Was this article helpful?