Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Detailed info about ID code usage in debugging w/ E10A-USB emulator.

Latest Updated:06/10/2011

Question:

I would like detailed information about how to use the ID code when debugging with the E10A-USB emulator.

Answer:

  1. When starting up after selecting the E10A-USB emulator mode (E10A-USB emulator startup mode)
    1. When you select “input new ID code” in the [ID Code] dialog box (checked) The flash memory is completely erased at startup. After it is erased, enter the ID code you entered when writing the program.
    2. When you do not select “input new ID code” in the [ID Code] dialog box (not checked): If the ID code you enter matches the ID code entered the previous time, the contents of the flash memory will be saved, and the E10A-USB will startup. Following this, the ID code you entered when writing the program will be written If the ID code does not match the previously entered ID code, the contents of the flash memory will be erased and the connection will be cancelled.

  2. When starting up after selecting the writing flash memory mode (flash memory data write mode)
    Data is written after all flash memory data is erased. There is no need to enter the ID code.
Suitable Products
E10A-USB