Skip to main content
Renesas Singapore - Knowledgebase

W0561016 Message_CC-RL

Last Updated:12/06/2017


I am using RL78 Compiler CC-RL. The following message is output. Why does this happen?
"W0561016:The evaluation version is valid for the remaining *** days"


This message is output because the CC-RL license key is not registered.
There is a 60-day trial period from the time of the first build. During the trial period, functionality is not restricted (as is the case with the evaluation edition). This message shows the remaining number of days.
After the trial period has expired, the link size is limited to 64KB, and the professional edition functions cannot be used.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?