Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Supported character codes_CA78K0R

Last Updated:02/28/2018

Question:

I am using a CA78K0R compiler for RL78.
When I tried to build after converting the character codes of a source file into UTF-8 code, building failed. Which character codes can be used with CA78K0R?

Answer:

The following character codes can be used.
-    SJIS code
-    EUC code
For CC-RL, UTF-8 can also be selected.
Suitable Products
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 and 78K Families
C compiler for RL78 Family and 78K0R[CA78K0R]