Skip to main content
Renesas Singapore - Knowledgebase

Reserved area for a compiler (CC-RL)

Last Updated:04/17/2017


I am using the CC-RL RL78 compiler. I have been using the CA78K0R compiler until now, and in that case the area from 0FFEB4H to 0FFEDFH was reserved for use by the compiler. Does CC-RL have a similar reserved area and, if so, what is the range?


No. CC-RL does not have a compiler-reserved area.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?