Skip to main content
Renesas Singapore - Knowledgebase

Requirement for Using Annual License

Last Updated:11/29/2017


I am considering purchasing an annual license.

Do I need to purchase a permanent license to use the annual license?


No, you do not.
Since the annual license and permanent license are independent licenses, you can use the annual license without the permanent license.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?