Skip to main content
Renesas Singapore - Knowledgebase

One Year Validity of Annual License Means

Last Updated:11/29/2017


It is written that annual licenses are valid for one year. Does this mean I can use the license for one year on the basis of actual compilation time?


No. It will expire on the date after one year from initial registration with the Renesas Web site of the code for obtaining the license which accompanies the compiler product.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family