Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

MCUs which can be used with the free evaluation edition (CC-RL)

Last Updated:06/14/2017

Question:

The free evaluation edition of RL78 CC-RL compiler can produce the sizes by linkage up to 64K bytes in total. Can it be used with MCUs of which on-chip ROM size exceeds 64K bytes?

Answer:

Yes, it can be.

In the evaluation editions, a restriction applies to the sizes produced by linkage (up to 64K bytes in total), but there is no restriction on MCUs of which on-chip ROM size exceeds 64K bytes.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?