Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Limit on the number of compiler packages with floating licenses

Last Updated:05/17/2017

Question:

Is there a limit on the number of compiler packages with floating licenses that we can install on a client PC?

Answer:

There is no limit on the number installed.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?