Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is the code it produces the same as that generated by the Standard edition?

Last Updated:05/17/2017

Question:

If I don’t use the features of the Professional edition, will the code it produces be the same as that generated by the Standard edition?

Answer:

Yes, it will produce the same code as long as the compiler has the same revision number.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family