Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

E0562321 message (CC-RL)

Last Updated:06/07/2017

Question:

I am using RL78 Compiler CC-RL. The following error message appears. How do I resolve this?

E0562321:Section "section-name-1" overlaps section "section-name-2"

Answer:

When an attempt to perform allocation by the linker is made, the "section-name-2" area overlaps the "section-name-1" area, and therefore this message appears.

Check the -start option of the linker or the address specification of the sections on the source file in the assembler description, and then change the specified location address so as not to overlap.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family