Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

E0562132 Message ".sdata"_CC-RL

Last Updated:02/21/2018

Question:

I am using RL78 Compiler CC-RL. The following error message appears. How do I resolve this?
"E0562132:Cannot find ".sdata" specified in option "rom""

Answer:

In the e2 studio and CS+ integrated development environments, the .data and .sdata sections for variables with initial values (output by default) are specified by default in the -rom option of the linker as sections to be mapped from ROM to RAM.

The E0562132 error occurred because the section specified in the -rom option did not exist.

Delete ".sdata=.sdataR" specified in the "Map from ROM to RAM" item of the link options of the e2 studio or CS+ integrated development environment.

However, note that if there is a variable with an initial value which is arranged in the saddr area during future development of programs, the value will not operate as expected unless ".sdata=.sdataR" is specified.

In the default startup routine, the size of the .sdata section is defined as 0.
 

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?