Skip to main content
Renesas Singapore - Knowledgebase

E0520095 Message(CC-RL)

Last Updated:04/17/2017


I am using the CC-RL compiler for RL78 devices. After defining a big array, I get the following message. How do I get around this? 
E0520095: Array is too large.
(Example) _far const unit8_t x[40000] = {


This message appears because the maximum value of bytes in a variable is 32767 by default.
You can increase this maximum value to 65535 by setting the -large_variable option.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?