Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Data filling for empty spaces (CC-RL)

Last Updated:05/10/2017

Question:

I am using RL78 Compiler CC-RL. How can I fill empty spaces with data?

Answer:

To fill empty spaces with data, you need to specify the range to fill.

In the settings of the linker, specify the output range by the -Output option and the value to be packed by the -Space option.

Note that if you use an IDE, the preceding output range should be specified by the division output file.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family