Skip to main content
Renesas Singapore - Knowledgebase

Creating DTC Vector Table for Specific Interrupt Source_CC-RX

Last Updated:11/22/2017


Does the DTC vector table need to be allocated to be assigned to all interrupt sources?

I also want to know how to make the table area smaller when only one interrupt source is used for DTC.


As specifying the DTC vector address to be used by #pragma address and setting the start address of the information to be transferred, the DTC table is created to only be assigned to the interrupt source specified.
Suitable Products
C/C++ Compiler Package for RX Family
  • Was this article helpful?