Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Compilers Supporting Annual License

Last Updated:11/29/2017

Question:

Do all compilers and versions support annual licenses?

Answer:

The following compilers and versions support annual licenses.

CC-RL: V1.01.00 and later

CC-RX: V2.03.00 and later

CC-RH: V1.02.00 and later

 

Note that only the above compilers and versions support annual licenses.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?