Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can I use licenses for Standard and Professional editions of revisions before the licenses were divided?

Last Updated:05/17/2017

Question:

Is it possible to use licenses for Standard and Professional editions of revisions before the licenses were divided in this way?

Answer:

Yes, you can use either license for old revisions.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family