Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Why can't I perform debugging using the watchdog timer function?

Latest Updated:01/16/2009

Question:

I cannot perform debugging normally when using the watchdog timer function in the debug system by the R8C UART Monitor Program. Why is this?

Answer:

For R8C/10-R8C/17 Groups, there is no watchdog timer refresh on the monitor of this debug system, and because of this a watchdog timer interrupt is generated and normal debugging cannot be carried out. Please do not use a watchdog timer in this system.
If you use other than R8C/10-R8C/17 Groups, there is watchdog timer refresh while the monitor is runnning. Please note that the watchdog timer is refreshed when the monitor is intervened by the operations such as a reference or change of the memory contents while the user program using a watchdog timer is running.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/10
R8C/11
R8C/12
R8C/13
R8C/14
R8C/15
R8C/16
R8C/17
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L