Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What should I do if an LCD display driven by an H8/300L faints?

Latest Updated:03/25/2009

Question:

What should I do if an LCD display driven by an H8/300L is faint ?

Answer:

There are two main reasons; if the LCD display drive voltage is low or the divided-voltage is variable, then it is not possible to drive the display correctly.

If the selected frame frequency is very fast, the LCD display may not be driven correctly due to a lack of driven capability.

Therefore, please adjust the driven-voltage and the value of frame frequency, taking into account the LCD panel performance.

Suitable Products
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power