Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What pin is required if the transmitter's TXD pin is set to N-channel ?

Latest Updated:10/10/2008

Question:

(Serial Interface)  When transmitting using asynchronous serial I/O (UART), if the transmitter's TXD pin is set to N-channel open drain output mode, what pin handling is required? [2008/10/10]

Answer:

An external pull-up resistor is required between TXD and the supply voltage. (#107149)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549