Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What makes H8S/26xx different from other H8S?

Latest Updated:03/18/2009

Question:

What is the most important difference between H8S/26xx and all other H8S ?

Answer:

H8S/26xx has a Multiply-Accumulate Unit (MAC) in its CPU. This aids DSP-type applications and also speeds up multiplications. It can execute a MAC in 200ns at 20MHz.
Suitable Products
H8S/2600
  • Was this article helpful?