Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What is the max bit rate to use in clock asynchronous serial I/O mode?

Latest Updated:02/27/2012

Question:

What is the maximum bit rate I can use in clock asynchronous serial I/O (UART) mode?

Answer:

In UART mode it operates by count source divided by 16, and so when the count source=f1, BRG=0, and CPU clock =24MHz (notes), it becomes 1.5Mbps at its fastest.

The formula is shown below:
f(XIN) / [(BRG+1) x Divided-by-16 x Count source dividing]

In addition, please meet the input setup time and the input hold time.

Notes: Since the maximum frequency of the CPU clock differs among MCUs, please refer to each data sheet.

Suitable Products
R8C/38A
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N