Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What is ADKEY function and are there any reference materials about it?

Latest Updated:08/05/2009

Question:

(A/D Converter)
What is the ADKEY function?
Are there any reference materials available regarding the ADKEY function? [2009/08/05]

Answer:

Similar to the key-on wakeup function, the ADKEY function is used to distinguish analog input voltage input from the ADKEY pin. When VIL (0.7 × VCC-0.5) or less is input, the A/D converter starts operating, and an A/D conversion interrupt can be used to distinguish analog voltage input.

For information on how to use the ADKEY function, please refer to the application notes below.

(#107429)

Suitable Products
38D2
38D5
  • Was this article helpful?