Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What instructions in H8S result in a performance increase over 300H?

Latest Updated:03/23/2009

Question:

What two instructions in the H8S instruction set result in a significant performance increase over the 300H?

Answer:

"LDM, STM. Load multiple and store multiple.

These 2 instructions allow the 300H to push and pop multiple registers onto and off the stack with one instruction. The H8S has to perform individual push and pop instructions for each register."

Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B
  • Was this article helpful?