Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What happens to the state of D/A converter if STP instruction was made?

Latest Updated:03/01/2005

Question:

(D/A Converter)  When the STP instruction is executed, what happens to the state of the D/A converter ? [2005/03/01]

Answer:

The D/A converter maintains output level even when the STP instruction is executed. (#104848)
Suitable Products
3803H
3803L