Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What's the reason why there's a 1 bit time when initializing the SCI?

Latest Updated:03/25/2009

Question:

When initializing the SCI, a waiting time of at least 1 bit is provided before TE bit or RE bit of Serial Control Register (SCR) is set to 1. What is the reason?

Answer:

The waiting period of 1 bit is the minimum time in order to initialize the internal state of SCI. If you don't wait the time before sending the data, erroneous data may be sent.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power